PDMM - Coordinated Motion Example with Ethernet/IP Interface to a Vision System
The attachments outline a KAS Application with the following features:
- 3 axis coordinated motion
- Banner vision camera connected to the PDMM via Ethernet/IP
- Camera reads a barcode and sends the information through Ethernet/IP to the PDMM.
- The bar code value is then used to determine which pattern to run
Home >
Knowledge Base >
FAQs >
Downloads >