Skip to main content

Kollmorgen Support Network

Operating Induction machines in AKD, using a closed-loop field oriented control | 06 Aug 2014 | |

Operating Induction machines in AKD, using a closed-loop field oriented control

Firmware version: M-01-12-01-000

This article explains how to set an AKD for driving an asynchronous machine, using a closed-loop field oriented control (FOC) strategy. The article contains:

Introduction

A Field Oriented Control (FOC) strategy to control an asynchronous machine is implemented in AKD. A separate control of flux and torque is possible, similar to a DC-machine. Fig 1 shows the implemented scheme.

ASM Close Loop FOC - Scheme.jpg

 

Figure 1: Field Oriented Control of an ASM

The velocity command can be obtained from three different sources, depending on DRV.CMDSOURCE

  • 0: Service
  • 1: Field bus
  • 3: Analog

Initial settings

DRV.OPMODE = 1  Velocity  mode
MOTOR.TYPE = 4      V/Hz speed control
FB1.SELECT = XX    Select according to your feedback
DRV.ACC & DRV.DEC  Set according to induction machine mechanical dynamics

Parameters

The following table shows which MOTOR parameters should be also configured for driving induction machines under FOC closed-loop operation:

Keyword

Induction Motor Closed Loop

Description

MOTOR.NAME

Yes

Set a name for customer motor

MOTOR.TYPE

Yes

Set to motor type. For V/Hz, MOTOR.TYPE = 4

MOTOR.AUTOSET

Yes

Available for FOC

MOTOR.IPEAK

Yes

Set to motor peak current (A).  150% of continuous current for NEMA motors

MOTOR.ICONT

Yes

Set to motor continuous current (A)

MOTOR.INERTIA

Yes

Set the motor inertia in kg cm2

MOTOR.KT

No

No necessary for Induction Motor

MOTOR.LQLL

Yes

Set the stator inductance in mH. For further information see below section “calculation of machine parameters”.

MOTOR.POLES

Yes

Set to motor poles 

MOTOR.VMAX

Yes

This is the maximum mechanical speed of the motor in RPM

MOTOR.R

Yes

Set the stator winding resistance phase-to-phase in Ohms. For further information see below section “calculation of machine parameters”.

MOTOR.VOLTMAX

Yes

Motor max winding voltage.  Ex: 230 VAC or 460VAC

MOTOR.PHASE

No

No necessary for Induction Motor

MOTOR.CTF0

Yes

This is used to configure the thermal constant of the motor coil

MOTOR.KE

No

No necessary for Induction Motor

MOTOR.IMTR

Yes

Set the rotor time constant in ms. For further information see below section “calculation of machine parameters”.

MOTOR.IMID

Yes

Set the magnetizing current (id) in A. For further information see below section “calculation of machine parameters”.

MOTOR.VOLTRATED

No

No necessary for FOC

MOTOR.VRATED

No

No necessary for FOC

MOTOR.VOLTMIN

No

No necessary for FOC

 

Field weakening.

So far, the closed-loop control implemented in AKD is not able to drive the ASM in field weakening area.

 

Calculation of machine parameters

Equivalent circuit.jpg

Figure 2: Induction motor equivalent circuit

     1. Determine current set point id = MOTOR.IMID

The direct-axis (non-torque axis) current Id is set to a constant value as soon as the drive is enabled. MOTOR.IMID is used to set up and view the magnitude of Id set point.

The appropriate value of MOTOR.IMID can be estimated from the motor nameplate information. 

A rule of thumb as follows can be used (see S300 manual):

Id.JPG

1

In which Id is the value for MOTOR.IMID, the preset rotor flux building current. IR and cos(phi)are the phase current and power factor at rated operation, read from the motor data sheet respectively. And 0.8 is an empirical factor. MOTOR.IMID is in Arms.

     2. Rotor resistance

The rotor resistance can be calculated based on the electrical motor losses. This means, based on the difference between ideal mechanical power and real mechanical power, the rotor resistance can be calculated as follows:

Rr.JPG

2

Where Pa is the ideal mechanical power, N0 is the synchronous speed and TeR is the nominal electromagnetic torque defined as:

Pa.JPG

3

No.JPG

4

TeR.JPG

5

PR, IR, fR and NR are the nominal values for power, current, frequency and speed, read from motor data sheet, respectively.

   3. Rotor inductance

The rotor inductance is defined as LR = Lm + Lró. Since Lm is bigger than Lró, we consider that: Lr = Lm. The mutual inductance can be calculated as follows:

Lm.JPG

6

    4. Rotor time constant

Finally, the rotor time constant is calculated as follows:

taoR.JPG 7

Vector current limiting

     1. Id limits:

  • Upper limit: 93.75% fold-back current limit, which is calculated as the smallest of drive current limit, motor current limit, and what fold back algorithm allows.
  • Lower limit: -93.75% fold-back current limit.

     2. Iq limits:

  • Upper: the lower of
    • Sqrt(Ifold^2 – Id^2)
    • User set Iq positive limit
  • Lower: the higher of
    • Sqrt(Ifold^2 – Id^2)
    • User set Iq negative limit

Commutation angle setting

For induction motor closed loop control the commutation angle is set as shown in the following figure:

Commutation angle setting AKD-IM.jpg

Figure 3. Commutation angle setting in AKD for IM

Induction motor close loop control supports using FB1 or FB2 as commutation feedback source.  The shaded calculation, adding motor position feedback to the slip, happens in the FPGA if using FB1 IL.FBSOURCE 0; and in firmware if IL.FBSOURCE is 1

Variables for analysis

Following variables are available for analysis and supervision:

IL.CMD

Currently reference for iq (torque-generation current)

IL.FB

Currently current for iq, at motor terminals

IL.IDCMD

Currently reference for id (flux-generation current)

VL.CMD

Velocity reference

VL.FB

Shaft position, read from the feedback

 

Further Information

Such concept is also implemented for our Servostar amplifier. You can find more information in the following links:

Induction Machine - General

Sensorless Control for Induction Machines with S300-S700

Operating Induction Machines S300-S700

 

Example

Considering the following ASM:

Nominal voltage = 230/460V

Nominal current = 8.75/5.05A

4 poles

Power: 2.20Kw

Nominal speed = 1395 rpm

 

cos(phi) = 0.82

Nominal frequency = 50Hz

 

 

With a resolver as feedback

Then, the missed machine parameters are calculated as follows:

  1. MOTOR.IMID:  based on equation 1:

Id2.JPG

  1. Rotor resistance.  The nominal electromagnetic torque is calculated based on eq. 5:

TeR2.JPG
    Based on eq. 4, we got the synchronous speed as:

No2.JPG

    The ideal mechanical power from eq. 3 is:

Pa2.JPG

    From eq. 2, the rotor resistance is then calculated as:

Rr2.JPG

  1. Mutual inductance. From eq. 6, we got:

Lm2.JPG

  1. Rotor time constant. Finally from eq. 7

taoR2.JPG

We set following parameters in AKD

Parameter

Value

Parameter

Value

DRV.ACC & DRV.DEC

10000rpm/s

MOTOR.POLES

4

DRV.OPMODE

1

MOTOR.VMAX

1600 rpm

FB1.SELECT

40

MOTOR.R

1.126 ohm

MOTOR.NAME

NORD-ASM

MOTOR.VOLTMAX

240V

MOTOR.TYPE

4

MOTOR.IMTR

114 ms

MOTOR.IPEAK

13 A

MOTOR.IMID

4 A

MOTOR.ICONT

8.75 A

 

 

MOTOR.INERTIA

6.2 kg cm2

 

 

MOTOR.LQLL

129 mH

 

 

 

Speed command: 1395 rpm

2014_08_06_09_50_112.png

Back to top

About this Article

juanramirez