The Basics of Selecting a Stepper Motor
The vast majority of stepper applications are fairly simple in terms of selecting the motor and drive. Most applications have one or more of a few criteria, usually including torque, speed,…
The P7000 was designed primarily for high inductance motors. The AC model has two ranges of inductance based on bus voltage, and the DC model has its own inductance range.
AC power (P70360):
160VDC bus - optimal motor inductance…
To enable the servo amplifier to also operate induction machines with the exact speed, the control structure had to be extended. For the additional elements, you must adjust the corresponding parameters.
In all sensorless modes, the output…
Firmware version: M-01-12-01-000
This article explains how to set an AKD for driving an asynchronous machine, using a closed-loop field oriented control (FOC) strategy. The article contains:
Firmware version: M-01-12-01-000
This article explains how to set an AKD for driving an asynchronous machine, using an open loop V/Hz strategy. The article contains:
General
A three-phase asynchronous machine (also called induction machine) can be used either as motor or as generator. It has a passive rotor, that is either is permanently (squirrel-cage rotor, cage rotor) or from case to case (dragging…