Skip to main content

Kollmorgen Support Network

Model Number: -NA vs -NB and -NC feature differences | 22 Nov 2014 | |

Model Number: -NA vs -NB and -NC feature differences

The label on the side of an AKD will indicate a model number. Each model number has extension -NA, -NB, or -NC. 

2014_11_21_23_11_022.png

Models with extension -NB or -NC support the following features which are not supported on -NA models.

  • Hiperface DSL and SFD Gen3 feedback types
  • Compare Engines
  • Tertiary feedback "Endat 2.2" over X9
  • Dual edge latching 
  • Multiturn overflow

-NA Hardware does not support firmware versions ≥ 01-15-00-001.

About this Article

Kollmorgen Support