For Kollmorgen (IDC) electric cylinders with a ballscrew and purchased with the "low temperature grease option", the special grease is Kollmorgen P/N 961266. This grease will be required for periodic maintenance of the actuator. …
The S600 drives built for sale in North America have a -550 suffix, e.g. S60301-550. These are all base drives with no option card installed. Kollmorgen - Radford will install the option card (if required) and re-label…
Industrial use of ever-faster and technically more complex servo drives in all areas of machinery, plant and equipment manufacture requires high-quality accessories.
No EMC problems, safe drive operation, Plug-and-Play are guaranteed with the…