Modbus TCP Communication Between AKD Drives and EXOR HMI Panels
Controlling AKD drives with HMI through Modbus TCP is easy but different panels need different adjustments.This article will help you in commissioning systems where you are using an EXOR Jmobile HMI panel and AKD drives.
After selecting the Modbus TCP protocol, you must add your AKD drive's IP address. Additionally, you should change the other settings to match, as is seen in the following screenshot.
The following screenshot shows some useful data addresses to control the AKD drive.
Lastly, please define the settings in order to read and write the parameters correctly. Change (swap) the data except for boolean parameters as shown in the following screenshot.
Following is a view from the panel test program, using an AKD drive.
Home >
Knowledge Base >
FAQs >
Downloads >