Skip to main content

Kollmorgen Support Network

Low Voltage AKD Operation | 02 Feb 2015 | |

Low Voltage AKD Operation

Numerous applications require lower than standard line voltages for a bushless servo application. The AKD can be ordered in a low voltage variant that allows for operation as low as 48 Volts DC. The part number for this variant is AKD-P00306-NBAN-0069  and has some special characteristics on the power scripts to allow for this operation.

In-rush ‘on’ threshold [VDC]

30

In-rush ‘off’ threshold [VDC]

15

Low regen threshold [VDC]

98

High regen threshold [VDC]

105

Over voltage level [VDC]

125

Under voltage level [VDC]

20

The DC bus voltage must at least reach 20VDC so as to not generate an under-voltage fault.

If applying DC power to the AC mains input terminals (L1 and L2), The DC bus voltage must at least reach 30VDC so that the in-rush relay will switch on.

Please see the following article regarding DC input power to the AKD drive: Using a DC Power Supply for AKD Bus Power | Kollmorgen

About this Article

Kollmorgen Support