Skip to main content

Kollmorgen Support Network

AKD2G Low Voltage DC Operation >

Table of Contents Overview Single Power Supply Operation.

EMC For Sevo Drives and Motors >

Troubleshooting EMI Noise and making EMC Compliance with Kollmorgen Drives.

Using a DC Power Supply for AKD Bus Power >

Many servo applications exist in which it is more practical to use a DC power supply for the motor bus power instead of using AC power.  Some of these include the use of batteries, generators, low voltage DC power supplies, and there are cases…

KCM Capacitor Module >

KCM modules (KOLLMORGEN capacitor modules) absorb kinetic energy generated by the motor when it is operating in generator mode (in the second and fourth quadrants; see Four Quadrant Operation). Normally, this energy is dissipated as waste via brake…

Building Power Supply Groups >

Since the failure rate of the servo amplifiers is very small, a line protection is sufficient from cost perspective. Further cost saving can be reached by group protection concept. If however a selective protection of the power supply is required…

Low Voltage AKD Operation >

Low voltage DC for AKD with 0069 option.

The Short Circuit Current Rating (SCCR) of the AKD Series Servo Drives >

The Short Circuit Current Rating (SCCR) of the AKD series servo drives is 42 kA.  

Fuses - Operation in UL-cUL Regions >

Valid for UL and CSA regions.

Fuses - Operation in CE Regions >

Table of Contents Power Supply Fuse Type 24V Supply Over current protection
Subscribe to Power and Fusing