Limiting AKD Velocity While In Torque Mode
Limiting AKD Velocity While In Torque Mode
Parameter IL.VLIMIT has been added to the AKD firmware to limit motor velocity while operating in torque mode. Setting it to a non-zero value will limit the velocity - in torque mode only - to the range of -IL.VLIMIT to IL.VLIMIT. The parameter IL.VLIMIT was released in firmware 01-14-04-00 beta on April 16, 2016
Home >
Knowledge Base >
FAQs >
Downloads >
Comments
Is there a simple issue that I am overlooking?
Thanks!