KVB Sample Projects for AKI Panels and AKD Drives (All versions of KVB)
This page contains links to the sample projects created in all versions of KVB.
These projects are for use in AKI panels connected directly to AKD servo drives and communicating over Modbus TCP. The AKI panel is the master and all AKD drives are slaves. These projects were NOT created for use with KAS.
KVB 2.20 software works with all CDA, CDB, CDC panels without having to do any firmware changes on those HMIs.
All 2.0 and 2.10 projects will have to be converted the first time they are opened in KVB 2.20. Once they have been converted to 2.20, they cannot be opened with the earlier versions. If you need to be able to revert back to KVB 2.0 or 2.10 to work with older panels, manually make a copy of the project directory folder before converting to version 2.20.
KVB 1.0 or 1.2 projects cannot be opened in version 2.0 or later. They also cannot be converted to the newer version. They would need to be re-created from scratch.
Version 2.20 SP2 Build 2.22.353.0
For AKD BASIC (AKD-T): https://kdn.kollmorgen.com/content/kvb-220-sample-project-aki-panel-and-akd-basic
For AKD Motion Tasking (AKD-P): https://kdn.kollmorgen.com/content/kvb-220-sample-project-aki-panel-and-akd-motion-tasking
Version 2.10 Build 2.15.2029.0
For AKD BASIC (AKD-T): https://kdn.kollmorgen.com/content/aki-panel-akd-basic-sample-project-indexing-kvb-210
For AKD Motion Tasking (AKD-P): https://kdn.kollmorgen.com/content/aki-panel-akd-motion-tasking-sample-project-cut-length-kvb-210
Version 2.0
For AKD BASIC (AKD-T): https://kdn.kollmorgen.com/content/aki-panel-akd-basic-sample-project-indexing-kvb-20
For AKD Motion Tasking (AKD-P): https://kdn.kollmorgen.com/content/aki-panel-akd-motion-tasking-sample-project-cut-length-kvb-20
Versions 1.0 and 1.2
For AKD BASIC (AKD-T): https://kdn.kollmorgen.com/content/aki-panel-akd-basic-sample-project-sprayer-kvb-10
For AKD Motion Tasking (AKD-P):
- Motion Tasking: https://kdn.kollmorgen.com/content/aki-panel-akd-sample-project-motion-tasking-kvb-10
- Simple Configuration: https://kdn.kollmorgen.com/content/aki-panel-akd-sample-project-simple-config-kvb-10
- Full Menu: https://kdn.kollmorgen.com/content/aki-panel-akd-sample-project-full-menu-kvb-10
- Cut to Length: https://kdn.kollmorgen.com/content/aki-panel-akd-sample-project-cut-length-kvb-10
Home >
Knowledge Base >
FAQs >
Downloads >