Skip to main content

Kollmorgen Support Network

KAS Application templates (Inside the IDE) | 17 Jun 2015 | |

KAS Application templates (Inside the IDE)

The KAS IDE includes a series of basic starter templates:

image

Templates are accessible in the IDE as follows:
   image

Then select a controller type:
   image

Then select a particular template:
   image

For details on each of these templates, see the IDE help file section "Project Templates"

For more advanced templates see the topic: Advanced KAS Project Templates

 

About this Article

C Wontrop