Skip to main content

Kollmorgen Support Network

EKM Motor Connectors and Corresponding Mating Connectors | 02 Dec 2014 | |

EKM Motor Connectors and Corresponding Mating Connectors

Kollmorgen does not offer power or feedback cables for the EKM series servomotors. Typically customer's will build their own cables for applications using the EKM motors.

The EKM motor connector part numbers are shown in the EKM Catalog (attached to this article).

The corresponding mating connectors are as follows:

Power

EKM2 and 3 – D38999/26FB5SN
EKM4 – D38999/26FC4SN
EKM5, 6, and 7 – D38999/26FE6SN

Feedback

ALL – D38999/26FB35SN

EKM_catalog.pdf (1.45 MB)

About this Article

josh.bellefeuille