KAS PxMM Controller Connected to a Control Logix PLC Through EtherNet/IP
This article is divided up into the following:
- Application note
- PDMM project
- Rockwell project
- PDMM EDS file(s)
This application note has two parts. Chapter 1 is an in-depth, step-by-step “how to” of adding Ethernet/IP communications to a KAS project as well as adding KAS support to a new or existing RSLogix5000 project. Chapter 2 is a hands-on quick start guide that explains how to upload the KAS EIP sample projects (.kas & .ACD files) in order to demonstrate correct setup / working Ethernet/IP communications.
Home >
Knowledge Base >
FAQs >
Downloads >