Changing Screens on the AKI Using a Modbus Register Value
From the Kollmorgen Visualization Builder under the list of System Tags there is a tag called New Screen ID and its definition.

If you click Add->System Tag in the Tag list, you can assign your desired Modbus address to it. The one shown is the one I used just for testing purpose so I could change the value using USER.INT1 in Workbench Terminal. Change it to the one you need for your case.

![]()
You’ll have to click on properties of each screen and assign each a Screen ID.
For example:

Note you will get an error if your Modbus register value is a Screen ID number that does not exist.
Home >
Knowledge Base >
FAQs >
Downloads >