Skip to main content

Kollmorgen Support Network

AKD Update rate - reading the motor temp sensor through SFD feedback | 08 Jun 2016 | |

AKD Update rate - reading the motor temp sensor through SFD feedback

What is the update rate in the AKD of reading the motor temp sensor through the SFD feedback?

Through the SFD feedback, the AKD monitors the motor temperature sensor  every 16 ms.  If the temperature sensor exceeds the maximum allowed temperature, a “301: Motor overheated” fault will occur on the AKD.

 

About this Article

C Wontrop