AKD MOTOR.BRAKE setting for low current brakes
In some application low current brakes are used which may cause the drive to fault on F305 Brake Open Circuit.
Cause:
Motor brake open circuit. Fault threshold is 200 mA.
Remedy:
Check cabling and general functionality.
For special low current brake applications, the F305 fault can be bypassed
using the setting MOTOR.BRAKE = 100 set via the Workbench terminal.
Once set, the brake state on the brake screen will show: 100-brake is fitted-fault ignored.
Home >
Knowledge Base >
FAQs >
Downloads >