AKD Motor without Temperature Sensor
The AKD has got the ability to use a third party motor without temperature sensor.
In this case the motor needs to be setup in the motor view. After this has been done the following two steps needs to be done:
- Within Workbench you need to select "no thermal sensor" within the view: Motor -> Motor temperature or in the terminal via: MOTOR.RTYPE 255
- Afterwards you need to deactivate the fault level for a temperature fault by setting MOTOR.TEMPFAULT 0 via the terminal.
Home >
Knowledge Base >
FAQs >
Downloads >