The utilization of robotics in manufacturing is currently a $5B industry and is projected to grow to a $20B industry (Source: A Roadmap for U.S. Robotics, From Internet To Robotics - 2013 Edition). A major contributor to the projected growth will…
Quick recap form our last post: In 1948, the company called Inland was formed by an out-of-work immigrant whose net worth was approximately $4000. Six employees ran the facility in the basement and garage of the Unruh home. The company's first…
There aren't many of us that open up the hefty manual that you receive with your new lawn tractor or dishwasher but if you did there would be a section in there on "preventative maintenance." There's a similar section in the documentation that comes…
Machine builders focus on functionality and reliability when first designing a new machine. Ideas are put on paper and components are strung together in block diagrams with thin lines to show the association of all the pieces. It is the most creative…
Coating and lamination applications demand
precise speed regulation in order to avoid velocity ripple that causes uneven
coating and undesirable horizontal bars across the substrate. The key to
achieving the most uniform coating is…
If you have been following along on our Evolution of Kollmorgen posts, you realize Hugo Unruh was one of the first to successfully commercialize frameless motor technology. What most people don't realize is that Kollmorgen's motor-drive phase…
A specification will often state the required stroke for the application. What is frequently seen is that units are damaged by not following a simple requirement stated in the Installation Manual. Best practices dictate the utilization of End of…
So up until now, we've seen how a couple of German immigrants came to America and turned their dreams into a reality. Fredrick came to America at the turn of the Century, Hugo a few decades later, and now Otto Kollmorgen had the reins of Kollmorgen…
Moore's Law has long applied to advancements in technology-based industries. Servo- and Automation have benefited particularly from exponential advancements in memory as well as processing power, and most recently, astounding gains in sensor…
Frequently, servo motors are returned where the brakes are worn. This is almost always due to the brake being applied repeatedly while the motor/load is moving. The application of a motor brake in a "dynamic / moving" scenario will result in dramatic…
There
is a nostalgic group out there thinking about when they first were introduced
to the BASIC language. BASIC? What is that? Kind of like today when
you say album or 45, or even vinyl – certain “younger” folk will look at you
and say…
Cogging and Torque Ripple questions are common and many times, difficult to answer.
Cogging torque is defined as the attraction/interaction of the magnetic poles to the teeth (steel structure) of the laminations within an un-energized motor.
Torque…