Hall Sensors
General
Hall Sensors (also called Hall encoders, accord. to Edwin Hall) uses the Hall effect to measure magnetic fields or electrical currents or positions.
If current flows through a Hall sensor and the sensor is placed in a magnetic field vertical to the current direction, the sensor delivers a voltage that is proportional to the product of magnetic field force and current. If the current value is known, the magnetic field force can be measured. If the magnetic field is produced by an electrical current in a conductor or coil you can do a potential free measurement of the electrical current in the coil.
A Hall sensor also delivers a signal if the magnetic field is constant. This is the decisive advantage compared to the combination of magnet and coil.
Applications
- Magnetic field measuring (magnetic flux density)
- Potential- free current measurement (current sensor)
- touch and contact free switches
- layer thickness measuring
In the car industry Hall sensors are used in the belt lock, in the door closing system, at the pedal state evaluation, in the gear control and in the ignition time measurement. Basic advantage is the insensitiveness against a non- magnetic dirt and water.
You can find them in "real" laser printers - in integrated circuits - to synchronize the mirror position, in disk drives, in brushless motors e.g. in ventilators. There are even keyboards with Hall sensors under every button.
Hall sensors with analog signal outputs are used for measurement of weak magnet fields (earth magnet field), for example with compasses in navigation systems.
They are used as current sensors in the gap of the iron core of a coil. Such current sensors are offered as a complete component, are very fast, can be used for DC measurement, too. They offer a potential separation between power and control circuits.
As position switch or contact free keypad they work combined with permanent magnets and have integrated a threshold switch.
Design
Hall sensors are produced out of thin semiconductor disks, because in these disks the number of electrons is small and therefore the electrons speed is high to reach a high Hall voltage. Typical designs are
- Rectangle
- Butterfly
- Cross
Usually the Hall sensors are integrated to the signal boost circuit or temperature compensation circuit.
Dimensions
The sensitivity is indicated in millivolt per Gauß (mV/G) with
1 Tesla = 10000 Gauß (1 G = 10-4 T).
Rotating Direction, Connection
Rotation clockwise (cw)


| Signal | Core Color | Other Description |
|---|---|---|
| H1 | (gn) | Signal a-b, phase U |
| H2 | (ye) | Signal b-c, phase V |
| H3 | (br) | Signal c-a, phase W |
With 5V power supply via X1 (S400:X2) observe the Sense line connections (pins 2 to 10 and pins 4 to 12).
Servo Amplifiers with Hall Support
| S300 | S400 | S601-S620 | S640/S670 | S700 | AKD | ||
|---|---|---|---|---|---|---|---|
| Connector for Hall | X1 | X2 | X1 -> Dongle | X1 | X1 |
Help for setup see page Setup of Hall Feedbacks.
Back to top
Home >
Knowledge Base >
FAQs >
Downloads >