Skip to main content

Kollmorgen Support Network

Fibre Optic | 07 Nov 2013 | |

Fibre Optic

General

Fibre optics are cables consisting or compound of light conductors, partly manufactured cables and lines provided with connectors for the transmission of light in the visible as well as ultraviolet or infrared range.

The transmission circuit consists of:

  • an optical transmitter,
  • a fibre optic cable, sometimes with repeaters (amplifying and signal generation)
  • an optical receiver.

these elements must fulfill the following requirements:

  • the optical transmitter must deliver a transmission power of –24 to –1 dBm.
  • the fibre optic cable must have a small damping/dispersion
  • the optical receiver must have a large sensitivity /typical -52dBm) and must be broadband.

Advantages

  • high transmission rate
  • high distance because of low damping
  • no crosstalk
  • no influence by outside electrical or electromagnetic perturbative fields
  • no grounding required

Disadvantages

  • Weak point plug technology
  • high manufacturing expenditure
  • relatively sensitive against mechanical load

Possible Disturbance

  • Damping by splices, inclusions, deformation of the core
  • Fibre break
  • Dispersion
Back to top

About this Article

Kollmorgen Support