Ana içeriğe atla

Search Articles

S300 Series Drive Connections for the Goldline B & M Series Motors S300 Motor Power Connector X9 S300  Power X9 Connector Pins İngilizce
S600 Series Drive Connections for the Goldline B & M Series Motors S600 Motor Power Connector X9 S600  Power X9 Connector Pins İngilizce
S700 Series Drive Connections for the Goldline B & M Series Motors S700 Motor Power Connector X9 S700  Power X9 Connector Pins İngilizce
FAQ PagesBelow are links to the various FAQs (Frequently Asked Questions) available on this site. İngilizce
PacSci SC900 & SCE900 Series Wiring Connections for the AKM Motors AKM Motor Feedback  Connector Functions SC900 & SCE900 Drive Feedback Connector İngilizce
PacCom Software Instruction Manual for 6445Software for 6445, 5345, 5445, 5645, SC150 & SC450.Requires true DOS computer. İngilizce
S300 and S600 Profibus Option CardsProfibus Option Card Labels: The Profibus option card for the S300 and S700 is labeled "Proibus DP".  (OPTION = H0Cxx) İngilizce
Using S300 virtual input to release motor brake via fieldbusThere is an undocumented parameter in the S300, SOFTIN. Bit 0 of this variable is for input 5, bit 1 for input 6,..., . If you set SOFTIN = 1, IN5 will return 1.To operate the brake set IN5MODE = 32.With SOFTIN = 1 the (virtual) input 5 is activated and the brake opens. İngilizce
Profibus Communication Rate and BandwidthProfibus Communication Rate and Bandwidth   The update rate of the Profibus communications is set in the Profibus master controller.  The GSD file of the drive allows a minimum time of 2ms. İngilizce