Salta al contenuto principale

Kollmorgen Support Network

Search Articles

Binary and Hexadecimal explanation and examplesFor those of us who need a periodic review of binary and hexadecimal numbers, here is a quick look. Decimal = Base 10 Binary = Base 2 Hexadecimal = Base 16     (4 Bits)    (1 nibble) Inglese
S300 CANopen velocity mode jogThis is a quick example and explanation of setting up and commanding a velocity mode jog move from CANopen. Inglese
AKM RoHS Compliance LetterAttached is the letter of compliance for All Standard Catalog AKIM Models represented by AKM1, AKM2, AKM3, AKM4, AKM5, and AKM7 comply to DIRECTIVE 2011/65/EU. Inglese
Servodisc Brush Replacement CommentsUnlike our other brush motor products, Kollmorgen does not sell replacement brushes for our Servodisc motors. Inglese
AKM Motor Shaft Seals (Teflon & Viton)This gives a brief overview of the teflon and viton shaft seals for the AKM product line.  The attachment contains the text listed in the below as well as some pictures of installed seals and 2D outlines of the seals. Inglese
Radford (R03) to Germany (D01) Accessories Cross ReferenceThis excel file contains many of the accessories sold in the U.S. and Europe.  Often the U.S. part number will coincide with the European standard of DE-XXXXX.  This file contains the part numbers that diverge from this standard. Inglese
AKD-N does not support secondary feedbackThe AKD-N (Near Drive) does not support secondary feedback (external encoder). There is a separate feedback connector on "DS" models, but that is for primary feedback only. There is no plan at this time to implement secondary feedback. Inglese
Decentralized Drive SystemThe AKD-C Power Supply and AKD-N drives lie at the core of a decentralized drive system. Up to 16 AKD-N drives can be connected to one AKD-C central power supply. Hybrid cables are used to connect the AKD-C to the drives and to daisy-chain the drives. Inglese
Coil Thermal Constant (MOTOR.CTF0)Calculating the coil thermal time constant for a motor based on the bulk motor thermal time constant. Inglese