Skip to main content
Success Story | 2 minute read

MULTI-SECTOR: FEED UNIT WITH DIRECT DRIVE LINEAR MOTORS

Direct Drive Absolute Value Unit

KOLLMORGEN linear motors in linear products made by Mondial

The head offices of MondialMachinery in a variety of industrial sectors has benefited from the properties, safety standards, compactness and precision of the positioning units driven by KOLLMORGEN linear motors.

Today, the well-known Mondial linear motor modules, long-established on the market, are more efficient and have higher quality standards, smaller dimensions, and an excellent price-quality ratio thanks to the compactness and safety of KOLLMORGEN products.

 

Mondial LogoMondial Spa is one of the foremost companies in the power transmission sector. For more than half a century, it has represented leading foreign companies, designing and producing a wide range of specialist products which can meet the most varied demands of many different industrial sectors. It is a parent company of the group of businesses specializing in the design and manufacture of specialist bearings for a number of different industrial applications. Boasting a design department, unusual feature for a distribution company, the Mondial Group works very closely with its clients to meet their needs, optimizing costs and benefits.

May 2014: Mondial needed to update and expand its range of modules driven by linear motors and upgrade the product design and performance in order to be able to offer customers a new and improved range of components in line with trends in the market as well as its own quality standards. The improved performance of the product has to be allied with the affordability of the proposed solutions; this was to be the key to success.

The Milan-based company began their search for a well-known partner in the market with which to operate in partnership. A meeting with KOLLMORGEN confirmed their interest in collaborating with a leading company capable of producing complete solutions. The result was a winning combination: both players immediately saw opportunities to increase their presence and competitive strength in the Italian market where the first applications combining the Mondial linear units with KOLLMORGEN linear motors were introduced at the start of 2017.

“The start of this partnership has been very exciting for us” explained Angelo Trombetta, Direct Drives and Mechanical Transmission Manager for Kollmorgen Italia, who has been with the project from the outset. “We have worked well with the Mondial team, mutual sharing has been useful and rewarding for all: this project has been a start, we want to tackle new challenges, continuing to provide the added value which is our hallmark”.

Complete linear movements with a high level of performance

Kollmorgen Mondial ICH Direct Drive Linear Motor Mondial uses KOLLMORGEN motors is its linear movement systems, which make up one of the most extensive ranges of direct drive linear modules on the Italian market. The benefits of direct drives are clear: very high performance, OEE (overall equipment efficiency) performance, no deterioration in performance over time, providing a transmission with maximum efficiency. The direct drive of a linear motor under load also means that mechanical transmission components, recirculating ball screws, gears, belts, and other components can be done away with, eliminating mechanical play, increasing rigidity and therefore productivity.

The linear units produced can be used in a wide range of machinery in applications such as printing, packaging, presses, plastic deformation, machine tools, handling, laser cutting, measurement, inspection, milling, assembly, textiles, simulators, and many more.

Transport and positioning unit MLM7 N

Kollmorgen Mondial Transport unit MLM7 NHigh levels of dynamic performance, considerable load capacity, and precision are the distinguishing features of the new MLM7 N series from Mondial. It is a complete feed and positioning unit, vital for linear movement in precision applications. The base component is made from high-strength extruded aluminium, which can be used as a free-standing element, the profile of which has been designed to suit different types of linear motors. It also provides high translation forces, whilst always ensuring fluidity of movement. The delivery programme, updated by Mondial, is structured in order to satisfy any application requirements in terms of speed, precision of positioning, load capacity, etc.

With regard to protection systems, the basic version has been designed with uncovered guide rails and protected recirculating ball slides with standard friction seals. The version with a linear motor has a stainless-steel plate to cover the motor. If the application requires, the MLM7 module can also be fitted with a PVC protective bellows. On request, Mondial can design and produce special protection systems to suit specific safety requirements or working environments. Maintenance is reduced to a minimum with this new range: the different versions incorporate a grease distribution system for all the moving components; the version with a linear motor uses lubricators integrated into the recirculating ball slides. The Mondial linear motor systems can also be fitted with inductive, magnetic, and optic linear encoders.

“KOLLMORGEN components provide the right solution for our manufacturing requirements, upholding the performance of our products and aligning with the quality requirements for the product and its quality certification”, commented Davide Torresan, Linear Systems Product Manager for Mondial Spa.

A direct drive linear motor is, in fact, a rotary engine laid flat and driven directly under load. With no mechanical transmission components, the design offers an exceptional level of performance, very high rigidity, dynamic speed, and acceleration, a high level of positioning precision, compact dimensions, low cogging, maintenance-free running, and quiet operation as well as a high degree of precision.

 
  • Advantages of the ICH linear motorsKollmorgen Mondial Direct Drive Linear Motor detail
  • Maintenance free, increased precision and bandwidth
  • Uniform speed profile and reduced noise
  • Transmission of forces without mechanical components such as couplings, toothed belts, etc.
  • No gear reducers, screws, or lubrication
  • Increased reliability of the application
  • Vast selection of motor sizes with differing power ranges for universal use in all linear drives
  • Increase in performance of the entire system
  • Compact drive solution with reduced height
  • Simple and more compact design of the machine
  • Increased bandwidth and response speed compared with ball screw or gear-wheel drives.
  • Reduced noise, fewer components and lower overall operating costs
 

Conclusion

In KOLLMORGEN, Mondial has not only found not only an excellent supplier but a genuine partner with which to offer both solutions in a complementary way: individual components and complete plug-and-play systems.

Kollmorgen Mondial Angelo Tormbetta, Direct Drive & Mechanical Transmission, KOLLMORGEN Italia

 

ABOUT KOLLMORGEN
Since the company was founded in 1916, the innovative solutions of Kollmorgen have formed the basis for big ideas, as well as improving the overall safety and quality of life of people. Kollmorgen offers continuous development of innovative solutions which are unrivalled in terms of performance, reliability, and ease of use. Crucial for this are valuable know-how of the drive systems and components sector, unmatched quality in the sector and substantial experience in combining and enhancing standard and customised products. We guarantee an unbeatable competitive advantage for machine manufacturers across the world with the highest possible safety standards for our customers. -- For more information, visit the website: www.kollmorgen.com

© KOLLMORGEN. Use for editorial purposes is free of charge.

Download as PDF

Direct Drive Linear Motors

Using Kollmorgen DDL direct drive linear motors, your machine can be simpler, faster, more precise and reliable. Pair your ironless, low profile or ironcore linear motor with an AKD or AKD2G servo drive for industry-leading power density.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights

High-Voltage Direct Drive Linear Motors Take Machine Tool Performance to New Heights >

IC Ironcore DDL linear motors and AKD servo drives delivered 65% greater positioning accuracy and 15% higher productivity for this double-faced grinding machine.
Direct Drive Linear Technology Enables Large-Scale Production of Calcium-Titanium Ore Solar Cells

Direct Drive Linear Technology Enables Large-Scale Production of Calcium-Titanium Ore Solar Cells >

Learn how a major solar-cell manufacturer significantly increased productivity and quality using high-performance, zero-cogging IL Ironless DDL direct drive motors.
Incorporating a Direct Drive Linear Motor into Your High Performance Machine

Incorporating a Direct Drive Linear Motor into Your High Performance Machine >

When mechanical designers use conventional servo motors to drive ballscrews or rollerscrews for linear motion, they quickly encounter limits to the speed and precision they can attain. Direct drive linear motors provide substantially higher…
Direct Drive Linear Motors Brochure

Direct Drive Linear Motors Brochure >

Kollmorgen offers direct drive linear motors to suit any application need. They’re fast, powerful, precise and maintenance-free. Our brochure has all the details.
Kollmorgen - 3D Cutting for large formats

3D Cutting for large formats >

Success Stories: Kollmorgen frameless direct drive linear motors for metal cutting
Servo solution for tube extrusion

Breyer - Kollmorgen servo solution for tube extrusion >

Servo solution by KOLLMORGEN: Clean cuts with linear motor and rotating blades.
Kollmorgen Direct Drive Linear Motor Catalog

Kollmorgen Direct Drive Linear Motor Catalog >

Catalog for Kollmorgen direct drive linear motors
Kollmorgen Automation and Motion Control - Full line catalog

Kollmorgen Full-line Catalog >

At Kollmorgen, we know that OEM engineers can achieve a lot more when obstacles aren’t in the way. With direct sales, engineering support, manufacturing facilities, and distributors spanning the Americas, Europe, the Middle East, and Asia, we’re…