What commutation offset do Kollmorgen motors have?
DBL / DBK with Encoder | Feedback has no defined commutation offset. The commutation offset is determined with the help of the servo amplifier and stored in the encoder memory. |
|---|---|
AKM with Hiperface encoder | Encoder is installed arbitrarily. The commutation offset is determined with the aid of the servo amplifier and stored in the encoder memory. |
AKM with BiSS encoder | Encoder is installed arbitrarily. Commutation offset is set to zero electronically. |
AKM with EnDat encoder | Commutation offset is mechanically set to zero. |
Home >
Knowledge Base >
FAQs >
Downloads >