Skip to main content

Kollmorgen Support Network

When does the fan run if a fan option card is built-in?

Fan on:
     Heat sink temperature > 65°C or environment temperature > 58°C or brake power > 30 Watts

Fan off:
    Heat sink temperature < 60°C and environment temperature < 55°C and brake power < 20 Watts