Skip to main content

Kollmorgen Support Network

What is the current supply at the SinCos encoder interface?

At connector X1 there are 5V/150 mA available. These values are nominal even at maximum load. If a higher current is required, we offer an external power supply (350 mA) with a 1m cable. See instructions manual.