Skip to main content

Kollmorgen Support Network

Shared Drive in PDMM or PCMM Application Fails to Mount | 24 Apr 2018 | |

Shared Drive in PDMM or PCMM Application Fails to Mount

The PxMM can work with data from an external or shared drive. Mounting is the software process in the PxMM that enables it to read and write data to/from a shared drive. If the mounting process fails in the PxMM the following message will appear in the IDE Controller Message Log.

Shared Drive failed to mount. ExitCode: 1, Message:Network configuration: Mount the shared directory gcode to /mount/shared

One common cause in a Windows 10 operating system is that the SMB1 was disabled. To enable it:

image   

Then:

image

For more information see: https://support.microsoft.com/en-us/help/2696547/how-to-detect-enable-and-disable-smbv1-smbv2-and-smbv3-in-windows-and

About this Article

C Wontrop