Is it possible to switch over parameters during operation?
Yes, either sequential with the function InxMODE=30 or with parallel switch over of two predefined parameter sets. Refer to page Switching over parameter sets.
Kollmorgen Support Network
Yes, either sequential with the function InxMODE=30 or with parallel switch over of two predefined parameter sets. Refer to page Switching over parameter sets.