I can't find my EnDat Motor in the motor database. What can I do?
Limit Ipeak and make sure, that no damage can occur even if the motor runs off.
Example 1: The motor type is not listed at all:
- Select FBTYPE = 4, SAVE, COLDSTART
- Read MPHASE, set MNUMBER = 0, SAVE; HSAVE and COLDSTART.
After rebooting, check MPHASE. If MPHASE no longer matches the original value, the source value must be set. Now all the motor parameters have to be determined.
Example 2: The motor is listed as a motor with resolver:
- Select FBTYPE = 4, SAVE, COLDSTART
- Read MPHASE, set MNUMBER = 0, SAVE; HSAVE and COLDSTART.
- FBTYPE = 0, SAVE, and COLDSTART. Then select the appropriate resolver motor and save with SAVE, then COLDSTART.
- FBTYPE = 4, SAVE and COLDSTART.
After rebooting, check MPHASE. If MPHASE no longer matches the original value, the source value must be set.
Home >
Knowledge Base >
FAQs >
Downloads >