An Example of How to Configure an AKD Motion Task Using ModBus
How to Configure a Motion Task using Modbus
MT.NUM 1 Modbus Address (548) MT.NUM command sets the Motion Task number being configured.
MT.LOAD Modbus Address (542) MT.LOAD command reloads the motion task parameters from the drive.
MT.ACC 1000 Modbus Address (526) MT.ACC command sets the acceleration to 1000 in the user units being used
MT.DEC 1000 Modbus Address (536) MT.DEC command sets the deceleration to 1000 in the user units being used
MT.V 100 Modbus Address (566) MT.V command sets the Velocity to 100 in the user units being used
MT.P 65535 Modbus Address (550) MT.P command sets the moves position to 65536 in the user units being used
MT.CNTL 1 Modbus Address (532) Motion Task Control Word is configuring the Motion Task as a relative move.
MT.SET Modbus Address (554) MT.SET command sets the Motion Task in the AKD drive
One Parameter or Multiple Motion Task Parameters Can be Configured using Modbus
MT.NUM 1 Modbus Address (548) MT.NUM command sets the Motion Task number being configured.
MT.LOAD Modbus Address (542) MT.LOAD command reloads the motion task parameters from the drive.
MT.V 500 Modbus Address (566) MT.V command sets the Velocity to 500 in the user units being used
MT.SET Modbus Address (554) MT.SET command sets the Motion Task in the AKD drive
How to Start the Motion Task:
MT.MOVE starts a motion task.
MT.MOVE 1 -> Start motion task number 1.
MT.MOVE 2 -> Start motion task number 2.
This command needs one argument in order to start a motion task. The drive must be homed, otherwise the motion task will not start (see also HOME commands).
Alternatively, MODBUS.MT can use used in place of MT.LOAD, MT.SET, and MT.MOVE.
Home >
Knowledge Base >
FAQs >
Downloads >