Skip to main content

Kollmorgen Support Network

DRIVE-CLiQ | 23 May 2016 | |

DRIVE-CLiQ

DRIVE-CLiQ is an open encoder interface. Kollmorgen offers AKM Motors with singleturn or multiturn Encoders and DRIVE-CLiQ Interface. The Motor feedback can be connected via an M12 connector to the SINAMICS drive System.

Temperature sensor type in the Motor is selected according to the current Siemens requirements.

About this Article

Kollmorgen Support