Does the setup software work with Debian Linux operating system?
The DriveGUI S300/S700 works with Linux Debian in the Windows Emulator WINE and communicates with the servo amplifier via the RS232 Com interface. An interface converter Ethernet or USB to RS232 is not required. An embedded PC has enough RS232 COM interfaces. So parameterizing, diagnostics and remote control can be done.
Home >
Knowledge Base >
FAQs >
Downloads >