WOOD DALE, IL – Danaher Motion has established the SynqNet Interest Group at SynqNet.org as an educational resource for design engineers to maximize the capabilities of the SynqNet technology in their performance motion applications.
Members benefit from full access to online and downloadable SynqNet articles, case studies, and flash animations, quarterly e-newsletters on the latest SynqNet news and developments, invitations to annual SynqNet meetings, and direct email access to SynqNet experts. Membership is free and is open to anyone interested in learning more about SynqNet. “With more than 270,000 axes running worldwide, SynqNet is the most widely utilized motion network in operation today and growing rapidly. As a result, the SynqNet Interest Group was established as an avenue of communication and education to help system and design engineers better understand the advantages of SynqNet system architecture and technology, and how it can help them build a better machine, faster, in performance motion control applications,” says Dean Onishi, SynqNet Communications Manager for Danaher Motion. Onishi says the group also aims to ensure ease-of-use and interoperability across SynqNet products for OEM’s and end-users. For more information or to become a member of the SynqNet Interest Group visit www.SynqNet.org. About SynqNet The SynqNet motion network utilizes the industry standard IEE802.3 physical layer for robust electrical isolation and 100 meter cable lengths with a deterministic protocol layer engineered by Danaher Motion. SynqNet was designed to meet demanding multi-axis motion applications and to address industry trends towards interoperable, digital machinery. SynqNet gives machines designers an open platform to meet the market demands for system modularity, HotReplace™ machine service without downtime, remote diagnostics, software field upgrade, multi-vendor support and fault-tolerant safety. Since 2003, more than 270,000 axes of SynqNet motion and I/O networking solutions have been installed. About Danaher Motion Danaher Motion is a leading global manufacturer of motion control products that improve the efficiency and productivity of complex manufacturing operations. Danaher Motion’s product innovations have been revolutionizing the motion control industry for over 60 years through trusted brand names including Dover, Kollmorgen and Thomson and Portescap.