Skip to main content

Kollmorgen Support Network

Fault Codes Amplifiers | 08 Aug 2008 | |

Fault Codes Amplifiers

Electronics
EA control circuitry EL logic inputs/outputs EV short-circuit/earth-short monitoring
EB regen circuit EM mechanics EW I²t monitoring
ED analog circuitry EN fan EX BTB/RTO signal circuit
EE output stage EP IPM output stage EZ DC-bus (DC-link)
EG basic p.c.b. / control card ER Feedback inputs EF no fault
EH aux. voltages ES SMPS EY other
EI current measurement ET driver stages    
EK custom print EÜ monitoring circuit    
Accessories
Z1 Option -01- ZE front panel ZR ROD 426 interface
Z2 Option -02- ZG 19" module/ compact case ZS SSI interface
Z3 Option -03- ZH case/housing ZT PROFIBUS interface
Z4 filter ZI keyboard ZU CAN interface
Z5 Option -RLG- ZK compact case ZV digilink
Z9 Option -CL- / -VL- ZL brake control ZW BIT CONNECT
ZA PC-interface ZM Display ZX PULSE CONNECT
ZB regen circuit ZN Encoder output ZF no fault
ZC resolver-digital converter ZO connector / terminals / cables ZY other
ZD DSP ZP backplane p.c.b. ZZ MODBUS interface
    ZQ SERCOS interface    
Component faults
ICs Adjustment and control components Electr. components + accessories
07 brake switch 20 trimmer pots 34 diode / zener diode
08 A/D- D/A converter 21 control pots 35 varistor / suppressor diode
09 PAL / GAL / CPLD / LCA 22 operating keys/buttons 36 FET
10 RAM Electrical connections 37 crystal oszillator
11 ROM / EPROM / EEPROM 60 connectors/terminals 38 capacitor
12 module / hybrid 61 solder joints 39 electrolytic ( also tantalum)
13 processor 63 screwed connections 40 resistor
14 interface components 64 links, short circuit 41 transformer
15 op-amp 66 track defects 42 inductance / coil
16 voltage regulator 67 bad contacting 43 shunt / power resistor
17 driver components 69 cable and other conductors 44 fuse
18 optocoupler Mechanical 45 fan
19 other ICs 73 bent / distorted / dented 46 relay
    85 paint / surface 47 DC-bus inrush circuit
Others Electr. components + accessories 48 transformer
97 wrong/missing packaging 30 LED 50 p.c.b. fault
98 no fault 31 power transistor 55 heat sink
99 Described Error not determined 32 transistor 56 front panel and fixing
00 other 33 rectifier    
Fault causes
General faults Customer faults Manufacturing faults
F part missing K0 autotransformer used H0 KVP
W mistaken/wrong part K1 connection fault H1 wrong component assembly
FF effective error K2 incorrect usage H2 assembly fault
M incorrect assembly K3 contamination H3 out of tolerance
D material defect K4 overheating H4 wrong module/ controller type
N no details K5 faulty application H5 wrong component
S other K6 attempted/faulty repair H6 coding, setting, basic adjustment
T transport damage K7 custom print missing H7 circuit diagram / component layout
UH hardware adaptation K8 corrosion / chem influences H8 other documents / nameplate
US software adaptation K9 other H9 other
PC Wrong program / parameter set        
Repair operations Procedure
Kollmorgen Europe GmbH R return W goods-inwards testing
S0 faulty repair U rebuild V precautionary
S9 other ER external repair X irreparable / scrap
SEE E replacement, Y other
A0 faulty repair EN - because irreparable V50 p.c.b. replaced
A9 other EV - precautionary, not ex-gratia    
Cost center
G warranty K fair dealing B to be invoiced

Note: If the fault designation OTHER is used, an additional description is always required.

About this Article

Kollmorgen Support