Ana içeriğe atla

Search Articles

Creating and Using a Recipe in KVB and AKI PanelA recipe can be used in an HMI program to store and select groups of data to be used without having to enter the data each time it is used.  It is easy to create a recipe in KVB by clicking on Insert / Recipe and give the recipe a name.  A recipe consists of Items and Data.  Each… İngilizce
EtherCAT Scan & Association - Adding Physical I/O SlicesThe following link points to an example from the KAS Online Help which shows how to add a physical I/O slice to an existing project. İngilizce
Analog I/O Parameters - I/O Terminals for Variable MappingThe following link points to an example from the KAS Online Help which discusses process data transferred to the Bus Coupler for variable mapping. İngilizce
EtherCAT Scan & Association - Couplers & I/O SlicesThe following page is an example from the KAS Online Help which shows how to add a coupler to an existing project. İngilizce
EtherCAT Coupler Error Handling And DiagnosisThe KAS IDE help has an extensive section on EtherCAT error handling.  İngilizce
KAS Support of AKT-SM-Lxx Stepper SlicesA topic from the KAS Online Help which discusses the support of AKD-SM-Lxx stepper slices by KAS. KAS Support of AKT-SM-Lxx Stepper Slices İngilizce
Using Homing Mode 17 With Single-turn and Multi-turn feedback TypesThis application note covers Homing Mode 17 in the AKD drive, how it works, and how to use it. İngilizce
IDC EC Series "Brake on Screw" OptionReplacement cable part number: 550-004  İngilizce
KAS Issue When Creating A New ProjectA crash can occur when creating a new project and there is no default printer selected on the PC. The workaround is  to set a default printer. Here is the procedure for selecting a default printer: 1. Click on the Start button and type Printers. İngilizce