Skip to main content

Whatever Happened to the Pacific Scientific PacSci Brand Motors?

All those permanent magnet DC motors, synchronous motors, servo motors, servo drives, stepper drives, oh yeah, and remember the great stepper motors they offered? The one stepper motor was a weird shape. It was octagonal where others are square or round. Hard to forget that one!

Good news! Kollmorgen recognized the great products Pacific Scientific offered and acquired them 15+ years ago. Up until November 2011 Kollmorgen maintained the Pacific Scientific branding and even after the acquisition, developed a few products that were branded Pacific Scientific. In November 2011 Kollmorgen announced that Danaher Corporation divested from the Pacific Scientific Aerospace business, which operated as a totally separate business from the Kollmorgen business. Included was the sale of the Pacific Scientific brand name and logo. As a result Kollmorgen removed all the Pacific Scientific branding and replaced it with Kollmorgen branding.

Many motor and drive families, formerly branded Pacific Scientific, are still available but are now branded Kollmorgen

PacSci Kollmorgen Motors

Former PacSci Products

Other Pacific Scientific products

The following motor and drive families, formerly branded Pacific Scientific are obsolete and no longer available.  You can find some manuals and technical documents in our discontinued products page and on the KDN Downloads page.

  • F Series servo motors
  • PMA servo motors
  • PMB servo motors
  • Regal / R Series servo motors
  • Sentry / S Series servo motors
  • PC3400 servo drives
  • SC320, SC400, SC100 servo drives
  • SC7xx, SC9xx, and PC8xx servo drives 
  • 5600 stepper drives
  • 62xx stepper drives
  • PD2400 stepper drive
  • BLF/BLR
 
POWERPAC® K and N -Hybrid Stepper Motor - Kollmorgen

POWERPAC K and N Series >

The POWERPAC series includes rugged NEMA 34 and 42 hybrid stepper motors designed to achieve extremely high torque. These units are available with standard options and co-engineered modifications to provide an exact application fit.

High TorquePOWERMAX II® M and P Stepper Motors - Kollmorgen

POWERMAX II® M and P Stepper Motors >

The POWERMAX II® M and P Series are NEMA 23 stepper motors feature an octagonal housing and are available in half-, single-, and two-stack configurations. These units offer a wide variety of standard options and affordable co-engineered modifications, without sacrificing scalability and lead time.

PMDC Motor - Kollmorgen

Permanent Magnet DC (PMDC) >

Our permanent magnet brush DC motors offer rugged, quality construction and dependable operation. Many options are available, including explosionproof models, washdown models, co-engineered modifications and more. With a well-deserved reputation for value, these motors are backed by a two-year warranty.