AKD Safety Characteristic Data
| Device | EN 13849-1 | EN 61800-5-2 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|
| Input STO-Enable | PL d, Cat.3 | SIL 2 | 1.50E-07 | 20 |
Don't know where to start?
Driving Aerospace & Defense Innovation with Motion Technology
Read MoreThis topic details the SIL CL, PFHD and TM safety characteristic data for servo components. This information is valid for AKD, S300, S600, S700, and AKM. Definitions for abbreviations may be found on the page Abbreviations.
The SISTEMA software utility provides developers and testers of safety-related machine controls with comprehensive support in the evaluation of safety in the context of ISO 13849-1. For S300 and S700 subsystems we offer a Sistema Library (see page Sistema).
| Device | EN 13849-1 | EN 61800-5-2 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|
| Input STO-Enable | PL d, Cat.3 | SIL 2 | 1.50E-07 | 20 |
| Function | Operation Mode | ISO 13849-1 | IEC 61508-2 | PFH [1/h] | TM [Years] | SFF [%] |
|---|---|---|---|---|---|---|
| STO | single channel | PL d, CAT 2 | SIL 2 | 1.88E-07 | 20 | 89 |
| STO | dual channel | PL d, CAT 3 | SIL 2 | 5.64E-09 | 20 | 87 |
| STO | dual channel with periodical testing | PL d, CAT 4 | SIL 3 | 5.64E-09 | 20 | 87 |
| Structure | STO | ISO 13849-1 | IEC 62061 | PFH [1/h] | SFF [%] | TM (Years) |
|---|---|---|---|---|---|---|
| AKD-C + 1 x AKD-N | global | PL d, CAT 3 | SIL 2 | 2.99E-08 | 97.08 | 20 |
| AKD-C + 8 x AKD-N | global | PL d, CAT 3 | SIL 2 | 3.07E-08 | 99.44 | 20 |
| 1 x AKD-N-DS | local | PL d, CAT 3 | SIL 2 | 2.9E-08 | 97.12 | 20 |
| Device | EN 13849-1 | EN 61800-5-2 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|
| Input STO-Enable | PL d, Cat.3 | SIL 2 | 1.50E-07 | 20 |
There is no certification for the S601-620 drives according to EN 13849-1 or EN 62061.
| Device S701-724 | Operation mode | EN 13849-1 | EN 62061 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|---|
| STO1/2-Enable | single channel | PLd, Cat.3 | SIL CL2 | 7.05E-08 | 20 |
| STO1-Enable+STO2-Enable | dual channel | PLd, Cat.3 | SIL CL2 | 7.05E-08 | 20 |
| STO1-Enable+STO2-Enable+STO-Status | dual channel with periodic test | PLe, Cat.4 | SIL CL3 | 1.04E-09 | 20 |
MTTF = 10 must be used in this case (according to the graduated process for estimation of MTTF in EN 13849-1:2008 chapt. 4.5.2). The motor encoder is already included in the characteristic data, so no further calculations need to be performed for the "Safe Actuator" subsystem. The subsystem is built from S700, safety card and motor feedback.
| Device (feedback with unknown MTTF) | EN 13849-1 | EN 62061 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|
| S700 with Safety card S1/S1-2 and unknown motor feedback | PL d, Cat.3 | SIL CL 2 | 1.26E-07* | 20 |
| S700 with Safety card S2/S2-2 and unknown motor feedback | PL d, Cat.3 | SIL CL 2 | 1.35E-07* | 20 |
* = depends on the MTTF value of the used feedback. The higher MTTF the smaller is PFHD . This has an influence to the complete system, even if PL and SIL classes don't change.
Most of the feedback systems, especially resolvers, have MTTF values larger than 57. The motor encoder is already included in the characteristic data, so no further calculations need to be performed for the "Safe Actuator" subsystem. The subsystem is built from S700, safety card and motor feedback.
| Device (feedback with MTTF > 57) | EN 13849-1 | EN 62061 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|
| S700 with Safety card S1/S1-2 and Kollmorgen motor feedback | PL e, Cat.4 | SIL CL 3 | 2.37E-08* | 20 |
| S700 with Safety card S2/S2-2 and Kollmorgen motor feedback | PL d, Cat.3 | SIL CL 2 | 1.35E-07* | 20 |
* = depends on the MTTFD value of the used feedback. The higher MTTFD the smaller is PFHD . This has an influence to the complete system, even if PL and SIL classes don't change.
In this case the system depends on the used feedback systems, therefore the system must be calculated individually. The given subsystem below is built from S700 and safety card S1-2, the feedback systems used by Kollmorgen are given as parts (see "Characteristic Data Feedback").
| Device | EN 13849-1 | EN 62061 | PFHD (1/h) | TM (years) |
|---|---|---|---|---|
| S700 with Safety card S1-2 | PL e, Cat.4 | SIL CL 3 | 1.19E-08 | 20 |
This is valid for drives with HWR >= 02.10.
| Device S748-772 | Operation mode | EN 13849-1 | EN 62061 | PFHD (1/h) | TM (Years) |
|---|---|---|---|---|---|
| STO1/2-Enable | single channel | PLd, Cat.3 | SIL CL2 | 7.05E-08 | 20 |
| STO1-Enable+STO2-Enable | dual channel | PLd, Cat.3 | SIL CL2 | 7.05E-08 | 20 |
| STO1-Enable+STO1-Status+ STO2-Enable+STO2-Status |
dual channel with periodic test | PLe, Cat.4 | SIL CL3 | 1.38E-09 | 20 |
| Device Safe Hiperface Encoder | EN 13849-1 | EN 62061 | PFHD (1/h) | TM (years) | MTTFD (years) |
|---|---|---|---|---|---|
| Safe HIPERFACE Encoder SKS36S/SKM36S | PLd, Kat.3 | SIL CL2 | 1.3E-08 | 20 | 847 |
Home >
Knowledge Base >
FAQs >
Downloads >