Skip to main content

Kollmorgen Support Network

MMG Cable sets | 19 Dec 2014 | |

MMG Cable sets

There are 2 different cable sets for the MMG, depending upon the encoder selection.  These cables are 10 feet long ( the "120" in the part number is length in inches).

MMG with digital encoder uses cable set 12-1414, which is comprised of 34237-120 power and 34236-00 feedback cables.

MMG with analog encoder uses cable set 34933-00, which is comprised of 34237-120 power and 34858-120 feedback cables.

12-1414.pdf (57.42 KB)
34237-120.pdf (170.31 KB)
34236-00.pdf (176.86 KB)
34933-00.pdf (48.28 KB)
34858-120.pdf (228.37 KB)

About this Article

Trevor Watson