Master/Slave FU/LU Roundoff with RATIO_GR and RATIO_SYN
This article refers to G&L PiC application note document AN000006 and describes Master/Slave, FU/LU roundoff with RATIO_GR and RATIOSYN.
When the feedback unit to ladder unit ratio specified for a slave axis is not a whole number, the magnitude of the numbers specifying the master and slave distances (MDST and SDST inputs to
RATIO_GR and RATIOSYN) has an effect on the actual master:slave ratio used. Internally, the FU to LU values are used to convert the MDST and SDST values from LU to FU. The resulting FU values are used to command a slave axis.
The equations are:
(slave FU * SDST) / slave LU = slave distance in FU
(master FU * MDST) / master LU = master distance in FU
where “/” represents integer division
Note the difference when specifying 1:1or 1000:1000 with MDST and SDST:
Slave FU = 10 actual slave distance used = (10 * 1) / 3 = 3 slave FU
Slave LU = 3 actual master distance used = (1*1) / 1 = 1 master FU
Master FU = 1
Master LU = 1
MDST = 1
SDST = 1
Slave FU = 10 actual slave distance used = (10 * 1000) / 3 = 3333 slave FU
Slave LU = 3 actual master distance used = (1 * 1000) / 1 = 1000 master FU
Master FU = 1
Master LU = 1
MDST = 1000
SDST = 1000
Note that in the first example the slave will move 3000 FU when the master moves 1000 FU. In the second example the slave will move 3333 FU when the master moves 1000 FU.
Also, when Master FU is less than Master LU, the magnitude of MDST will determine whether or not a master distance is accepted. For example:
Master FU = 1 actual master distance used = (1 * 1) / 5 = 0 master FU
Master LU = 5
MDST = 1
SDST = 1
Master FU = 1 actual master distance used = (1 * 10) / 5 = 2 master FU
Master LU = 5
MDST = 10
SDST = 10
Note that the computed master distance in the first example is 0. This will result in an “Invalid Master Distance” error despite the fact that MDST = 1.
Home >
Knowledge Base >
FAQs >
Downloads >