Coating and lamination applications demand
precise speed regulation in order to avoid velocity ripple that causes uneven
coating and undesirable horizontal bars across the substrate. The key to
achieving the most uniform coating is…
If you have been following along on our Evolution of Kollmorgen posts, you realize Hugo Unruh was one of the first to successfully commercialize frameless motor technology. What most people don't realize is that Kollmorgen's motor-drive phase…
A specification will often state the required stroke for the application. What is frequently seen is that units are damaged by not following a simple requirement stated in the Installation Manual. Best practices dictate the utilization of End of…
So up until now, we've seen how a couple of German immigrants came to America and turned their dreams into a reality. Fredrick came to America at the turn of the Century, Hugo a few decades later, and now Otto Kollmorgen had the reins of Kollmorgen…
Moore's Law has long applied to advancements in technology-based industries. Servo- and Automation have benefited particularly from exponential advancements in memory as well as processing power, and most recently, astounding gains in sensor…
Frequently, servo motors are returned where the brakes are worn. This is almost always due to the brake being applied repeatedly while the motor/load is moving. The application of a motor brake in a "dynamic / moving" scenario will result in dramatic…
There
is a nostalgic group out there thinking about when they first were introduced
to the BASIC language. BASIC? What is that? Kind of like today when
you say album or 45, or even vinyl – certain “younger” folk will look at you
and say…
Cogging and Torque Ripple questions are common and many times, difficult to answer.
Cogging torque is defined as the attraction/interaction of the magnetic poles to the teeth (steel structure) of the laminations within an un-energized motor.
Torque…
The American Meat Institute generated a Fact Sheet related to Sanitary Equipment Design in 2008 which helps the OEM Machine builder to design sanitary solutions for the Food Processing and packaging market. Our blog post looks at the 10 sanitary…
Washdown applications can be quite the tough environment. In the first place, typically you’ll find washdown requirements on machines that process foods. You know how careful you are when cooking at home, making sure you wash your hands after…
Consumers expect safe food. The Feds expect a safe food supply chain-farm, processing, packaging, and distribution. As we all work to consistently meet consumer food safety expectations, the need to prevent and control food adulteration…
When a load is driven directly by the motor, the conversation around reflected inertia goes out the window. The belief is that direct driven loads do not, by their nature, have a reflected inertia. Some folks are even confident enough to say that the…