A motion controller is a programmable device that manages connected electronic drives and motors to perform specific functions for automating and controlling machinery. Motion controllers can range from very simple microprocessor chips embedded…
If you experience some unintended motion or unexplained drive faults in your motion system, there are several possible causes. For example, motion setup through the drive, a poorly designed program within the control, and motor or feedback…
Servo systems are widely used in many precision applications. While careful deliberation on the optimum servo motor, servo drive, and feedback elements is the norm, the cables that connect the power and feedback are often an afterthought that…
While servo motors and drives are prevalent in a wide variety of industrial applications, what should be considered when they operate in extreme or hazardous environments? In many cases, the motor itself operates in the extreme environment, while the…
How do I calculate a motor’s continuous torque when it is operating in an environment above its rated temperature? Since the motor’s continuous torque (Tc) is rated in a 40°C ambient, how can I estimate the motor’s continuous torque during my…
Machine Learning, Neural Networks – big terms in modern logistics, but what do they actually mean? What we need is an expert to tell us. Paul Hamblin, editor of Logistics Business magazine, meets one.
Using a conventional single motor and gearbox style setup on your horizontal flow pack machine could be the reason you’re not realizing the flexibility and performance you need to keep up with demand.
For manufacturers looking to offer personalization capabilities, true mass customization to batch size of one will require more than purchasing the latest 3D printer or equipment. It’s important to understand the entire supply chain involved,…
When and how to customize a standard servo motor depends on the predicted benefits derived from the customization that should include a solution tied to form, fit, and function. Learn more.
An alternative to customizing a servo motor is utilizing a frameless motor and integrating directly into the machine itself. Learn more in our new blog post!
There are lots of reasons to choose a frameless motor. They’re extremely compact, simple, efficient and precise. Is that what your application requires?
An explosion proof motor is clearly marked with a nameplate that identifies its suitability for a given hazardous environment. The nameplate will indicate the hazardous Class, Division, and Group for which the motor is suited.
Electric motors generate heat under normal operating conditions and have the potential to generate a spark if a motor coil fails. Excessive motor case temperatures or a spark that is not properly contained can cause an explosion or ignite a fire in…
From concept to production, Kollmorgen is the one partner you need for the most ambitious design, the most capable engineering and the most confident delivery.
Electro-optical/infrared systems play a crucial defense role on land, in the air, at sea and in space. See how we engineer motion solutions to help you make every design mission a successful one.