Pular para o conteúdo principal
Histórias de Sucesso | Leitura de 2 minutos

Optimizing Bottle Production

Kollmorgen Solution Catapults PET Bottle Blow Molding Machine to Top Producer in the World

Challenge

A major bottling operation in China needed to substantially increase output in order to ensure future success in a highly competitive market. For the company’s all-electric linear PET bottle blow molding machine, productivity depends on the ability to quickly index PET preforms into position and then remove the resulting molded bottles. The company engaged Kollmorgen motion experts in early 2019 to help minimize the machine’s indexing time.

Working closely with the customer’s machine design team, Kollmorgen engineers discovered that the indexing performance requirements were overtaxing the existing motor/drive solution. The motor wasn’t able to achieve the desired indexing speed without overheating. The drive was unable to supply the necessary acceleration current and would quickly go into current foldback, further limiting the power needed to meet the desired indexing time.

The only way to prevent overheating and foldback in the existing motor/drive combination was to increase the indexing time – slowing the machine down to the point that bottle-production targets could not be met. While a larger motor might have solved the problem, the machine design was fixed and did not provide the additional space that would be needed.

Solution

Achieving faster indexing times would require more acceleration torque and lower overall inertia. Kollmorgen worked closely with the customer to evaluate the indexing goals and to co-engineer a solution that would deliver the desired machine performance improvements. A Kollmorgen 2G Motion System supplied the additional power needed to dramatically decrease index time while occupying the same space as the prior motor and drive design.

Results

A simple, cost-effective upgrade to the 2G Motion System transformed the PET bottle blow molding machine and reinvigorated the customer’s business.

  • Motor torque increased by 30% without an increase in size.
  • Faster acceleration reduced the indexing time from 1.6 seconds to 1.3 seconds, a 23% improvement.
  • No machine modifications were required to fit the AKM2G servo motor onto the existing motor mount, saving the customer design and documentation time.
  • The machine now produces 156,000 bottles (600 ml) per hour, making it the #1 bottle producer in the world.

“This is what the 2G product was designed for —increasing the performance of our customer’s machine without taking away precious space for a larger drive and motor.” - Tom Kunkel, 2G Product Manager, Kollmorgen

Learn more

Ready to discover what the 2G Motion System can do for your machine?

Learn more

 

About Kollmorgen

Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives. Today, its world-class knowledge of motion systems and components, automated guided vehicle navigation software, industry-leading quality, and deep expertise in linking and integrating standard and custom products continually delivers breakthrough motion solutions that are unmatched in performance, reliability, and ease of use. This gives machine builders around the world an irrefutable marketplace advantage and provides their customers with ultimate peace of mind.

Movimento pronto para usar impulsiona o robô de resolução de cubos mais rápido de todos os tempos

Descubra como um sistema de movimento pronto para usar impulsionou o robô de resolução de cubos mais rápido. Velocidade, precisão e movimento multieixo sincronizado explicados.

Learn More

Amplificadores de servodrives CA PM: diferentes alinhamentos de fase e comutação do servomotor

Os problemas para alinhar a comutação entre servomotores e servodrives, especialmente quando o motor e o drive são de fabricantes diferentes, podem ser bastante desafiadores. Entender os desafios típicos de projeto pode ajudar a lidar com problemas de sequenciamento de fases do motor.

Learn More

Engenharia excepcional

A Kollmorgen acredita no poder do Motion Control e da automação para construir um mundo melhor.

Descubra Mais

Recursos Relacionados

Equipamentos de soldagem de baterias de lítio

A segurança funcional dos motores lineares aprimora a segurança e a produtividade em equipamentos de soldagem de baterias de lítio >

A tecnologia de segurança funcional SMM da Kollmorgen ajuda a alcançar movimentos estáveis e controlados, além de conformidade global para a produção e competitividade de baterias de lítio.
instalações de fabricação com controle de movimento multieixo

Como dominar o controle de movimento multieixo em células de produção modernas >

Quando os sistemas de movimento escalam, a sincronização se torna mais difícil. Saiba como as células de produção modernas mantêm a precisão, a estabilidade e a produtividade em alta velocidade.

Movimento pronto para usar impulsiona o robô de resolução de cubos mais rápido de todos os tempos  >

Descubra como um sistema de movimento pronto para usar impulsionou o robô de resolução de cubos mais rápido. Velocidade, precisão e movimento multieixo sincronizado explicados.
Como o sistema de movimento da Kollmorgen aciona um robô a cabo para triplicar a produtividade

Como o sistema de movimento da Kollmorgen aciona um robô a cabo para triplicar a produtividade >

Saiba por que a Rbot9 especificou servomotores AKM2G e servodrives AKD para maximizar a capacidade de carga, a velocidade e a segurança de carga vertical de seu imenso robô suspenso por cabos.
Amplificadores de servodrives CA PM: diferentes alinhamentos de fase e comutação do servomotor

Amplificadores de servodrives CA PM: diferentes alinhamentos de fase e comutação do servomotor >

Os problemas para alinhar a comutação entre servomotores e servodrives, especialmente quando o motor e o drive são de fabricantes diferentes, podem ser bastante desafiadores. Entender os desafios típicos de projeto pode ajudar a lidar com problemas…
Sessões de mentoria do AKD2G: guia de configuração rápida do AKD2G

Sessões de mentoria do AKD2G: guia de configuração rápida do AKD2G & configuração avançada para AKD2G de eixo duplo >

Precisa começar a trabalhar com seu novo sistema 2G? Tudo começa com o software AKD2G Workbench. Esta sessão fornecerá os fundamentos necessários para criar motion rapidamente, construir confiança e acelerar sua produtividade.
Segurança funcional 101 WP

Segurança funcional 101: o que? por que? e como?  >

Mesmo para empresas com sede nos países em que não haja exigência de normas de segurança funcional, é provável que vários de seus clientes exijam equipamentos que estejam em conformidade. Desde proteger funcionários e reputações até melhorar a…
A Kollmorgen ajuda o fornecedor de soluções de automação de embalagens  a atender à necessidade de embalagens sob demanda “com o tamanho certo”

A Kollmorgen ajuda o fornecedor de soluções de automação de embalagens a atender à necessidade de embalagens sob demanda “com o tamanho certo” >

A experiência da Kollmorgen em componentes de controle de movimento para linhas de embalagem ajudou a Packsize a enfrentar desafios exigentes para criar soluções de automação de embalagens revolucionárias.

Como começar a dimensionar e selecionar servos: entendendo a necessidade de uma solução para seu sistema >

Dimensionar e selecionar um sistema de servomotor para um projeto de máquina começa pela compreensão dos componentes que formam um servomotor ou sistema de servoacionamento. Os sistemas de servo são de malha fechada, para controle algum movimento…