Many applications require a number of axis so high that it's not possible to use one PCMM only.
In order to get over this limitation it's possible to use more controllers with the benefits of exchanging data between them.
There are three chances…
There are three types of Profinet telegrams for use with the AKD drive:
Standard Telegrams
Manufacturer Specific Telegrams
Free-mappable Telegram (400)
The Standard Telegrams and Manufacturer Specific Telegrams are pre-configured telegrams with…
This page provides information and downloads related to TIA Portal sample projects for Profinet communication between the Siemens S7 PLC's and AKD Profinet drive.
The sample projects use a function block to handle the telegram data and state…
Hi guys,
right now I am working at a app, where are PLC S7-1214C and two servos AKD-P00307-NBPN-E074. There is communication by profinet. Unfortunately PLC is not able connect to AKD servos via profinet. PLC doesn't see both AKD servos. I had checked…
The system covered includes a PxMM controller with up to twelve additional AKD drives.
All automation functions are handled in the PLC, the functionality covers the following: