Skip to main content

Kollmorgen Support Network

Servo Drive WorkBench GUI Standard Setup EN

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD and AKD2G devices. For more information regarding features, see the AKD WorkBench Release Notes.

File Versions

Kollmorgen-WorkBench-2.20.0.12468-Setup-English.exe_.zip (531.29 MB)
2.20.0.12468

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. Supports AKD, AKD2G, KED, and MKD devices. For more information regarding features, see the Workbench Release Notes. English-only GUI. This release introduces support for Kollmorgen Essentials and the KED. 

Kollmorgen WorkBench 2.19.0.11951 Setup English.exe_.zip (513.98 MB)
2.19.0.11951

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes full installer: the application with complete help files and the .NET Framework required by the application. Supports AKD, AKD2G, KED, and MKD devices. For more information regarding features, see the Workbench Release Notes. English-only GUI. This release introduces support for Kollmorgen Essentials and the KED. 

2.17.0.10918

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

2.16.0.10497

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Kollmorgen WorkBench 2.14.0.9656 Setup English.exe_.zip (290.76 MB)
2.14.0.9656

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Kollmorgen_WorkBench_2.13.0.9674_Setup_English.exe_.zip (310.89 MB)
2.13.0.9674

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD, AKD2G, and MKD devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Kollmorgen WorkBench 2.12.0.8547 Setup English.exe_.zip (236.76 MB)
2.12.0.8547

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD and AKD2G devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Kollmorgen WorkBench 2.13.0.9149 Setup English.exe_.zip (287.78 MB)
2.13.0.9149

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD and AKD2G devices. For more information regarding features, see the AKD WorkBench Release Notes. English-only GUI.

Kollmorgen WorkBench 2.11.0.8192 Setup English.exe_.zip (217.15 MB)
2.11.0.8192
REV 2.11.0.8192

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. Supports AKD and AKD2G devices. For more information regarding features, see the AKD WorkBench Release Notes.

Kollmorgen WorkBench 2.10.0.7363 Setup English.exe_.zip (201.57 MB)
2.10.0.7363
REV 2.10.0.7363

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Full Setup EN (2.9.0.6662).zip (339.2 MB)
2.9.0.6662
REV 2.9.0.6662

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Setup EN (REV 2.8.0.6350).zip (167.61 MB)
2.8.0
REV 2.8.0.6350

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Standard Setup EN (REV 2.7.0.5821).zip (150.08 MB)
2.7.0
REV 2.7.0.5821

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

Kollmorgen Servo Drive WorkBench GUI Standard Setup EN (REV 2.6.0.5516).zip (162.35 MB)
2.6.0.5516
REV 2.6.0.5516

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD2G Servo Drive WorkBench GUI Standard Setup EN (2.3.0.4870).zip (136.1 MB)
2.3.0.4870
REV 2.3.0.4870

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

Kollmorgen Servo Drive WorkBench GUI Standard Setup EN (REV 2.2.0.4448).zip (120.65 MB)
2.2.0.4448
REV 2.2.0.4448

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Standard Setup EN (REV 2.1.0.3945).zip (101.04 MB)
2.1.0.3945
Rev 2.1.0.3945

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

Kollmorgen WorkBench 2.0.0.3088 Setup English.zip (64.57 MB)
2.0.0.3088
Rev 2.0.0.3088

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Standard Setup EN (REV 1.18.0.2828).zip (52.61 MB)
1.18
REV 1.18.0.2828

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench Standard Setup EN (REV 1.18.0.2766).zip (52.61 MB)
1.18
REV 1.18.0.2766

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from the internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Standard Setup EN (REV 1.17.0.2215).zip (40.76 MB)
1.17
REV 1.17.0.2215

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive WorkBench GUI Standard Setup EN (REV 1.17.0.1599).zip (35.67 MB)
1.17
REV 1.17.0.1599

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes

AKD Servo Drive WorkBench GUI Standard Setup EN (REV 1.16.0.41).zip (37.16 MB)
1.16
REV 1.16.0.41

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

AKD Servo Drive GUI Standard Setup EN (REV 1.15.0.27).zip (36.26 MB)
1.15
REV 1.15.0.27

WorkBench is a Graphical User Interface that allows configuration from different Kollmorgen devices. Includes standard installer: the application with complete help files. The .NET Framework is downloaded from internet if not already installed. For more information regarding features, see the AKD WorkBench Release Notes.

About this Download