North America
|
RADFORD, VA – August 28, 2019 – Attendees of the AUSA 2019 Annual Meeting & Exhibition in Washington, DC, October 14 -16, are invited to visit Booth #7619 to meet Kollmorgen aerospace and defense experts and learn more about the company’s motion solutions for applications including: EO/IR, remote weapon stations, military robotics, radar satcom systems, missiles and guided munitions, and other high-performance systems.
“As part of the industry for the past 100 years, Kollmorgen has worked with all the major defense OEMs around the world to help innovate in a wide variety of applications,” said Mike Crowe, Director of A & D. “Kollmorgen motors are found on the floor of the ocean, on the surface of Mars, in outer space, as well as in mission-critical land, sea and air applications.”
Kollmorgen combines its core motion control expertise with award-winning motion technologies – direct drive servo motors, brushed and brushless torque motors, servo and stepper motors, linear actuators, gearboxes, and controls – to create the most advanced aerospace and defense applications, including the following:
Electro-Optical/Infrared(EO/IR): Kollmorgen provides motor technology that enables smooth, accurate, and stable motion to position image sensors and long-range detection systems. These rugged motors are directly coupled to the internal workings of the EO/IR system to provide the visual integrity and stability required for even the most extreme conditions.
Military robotics: Kollmorgen has been on the leading edge of precision robotics technology for decades with over 100,000 units fielded in high-reliability systems. Award-winning TBM™ frameless motors are optimized for fit and performance with industry standard strain wave gearing and industry-leading torque density to enable precise, smooth, reliable motion for defense applications including bomb-disposal robots.
Remote weapons stations: Kollmorgen’s compact, lightweight KBM™ frameless servo motors excel in meeting the extreme multi-axis torque and speed requirements for remote weapons stations.
Radar satcom systems: Kollmorgen’s TBM™ frameless motors deliver the torque required for the rapid acceleration and deceleration needed for radar and antennas with substantial mass, while maintaining accurate positioning.
Learn more about Kollmorgen in this video: Kollmorgen – A Century of Innovation in A&D.
ABOUT KOLLMORGEN
Since its founding in 1916, Kollmorgen’s innovative solutions have brought big ideas to life, kept the world safer, and improved peoples’ lives through its world-class knowledge of motion systems and components, automated guided vehicle software, and industry-leading quality. Kollmorgen’s deep expertise in linking and integrating standard and custom products continually delivers breakthrough motion solutions that are unmatched in performance, reliability, and ease-of-use. Kollmorgen solutions give machine builders around the world an irrefutable marketplace advantage, while providing their customers with ultimate peace-of-mind.
For more information call 1-540-633-3545.