Profinet Real-Time Jog in AKD vs. AKD2GThe Real-Time Jog feature in Profinet allows the PLC to change the jog speed, acceleration, deceleration, and direction on the fly (while the jog motion is active). The following telegram data is used for the Real-Time Jog: |
jcoleman02 |
English | |
AKD2G Profinet Landing PageThis application note demonstrates AKD2G parameter access from a S7-1500 PLC using the SinaPara function block for multi-parameter access and the SinaParaS for single parameter access. |
toddevans01 |
English | |
Establishing Commutation for Encoder-Halls Based Motors with the AKD/AKD2GCommutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases. If the rotor position of the motor is not determined correctly or the motor power phase wires |
jcoleman02 |
English | |
Establishing Commutation for Resolver Based Motors with the AKD/AKD2GCommutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases. If the rotor position of the motor is not determined correctly or the motor power phase wires |
jcoleman02 |
English | |
AKD CANopen Cheat SheetThe attached Excel spreadsheet provides quick look up charts and explanations grouped by topics and tabs for AKD1G CANopen communications. |
toddevans01 |
English | |
AKD EtherCAT and CANopen Torque ScalingThe following summarizes the 2 types of torque scalings for AKD1G EtherCAT and CANopen. See the attached document for a full application note. |
toddevans01 |
English | |
AKD EtherCAT and CANopen Landing PageThis landing page contains links to other articles and downloads relating to AKD EtherCAT and CANopen communication. |
jcoleman02 |
English | |
KAS Stepper Control with AKT2G slicesAKT2G-SM-L50-000 and AKT2G-SM-L15-000 EtherCAT stepper drives allow you to control Stepper motors up to 5 Amp (6.5 with fan cartridge AKT2G-AC-FAN-001) with a PDMM or PCMM controller. | Joe Parks |
English | |
HMI Operating System VersionsThe HMI displays the Windows Embedded version in the lower-left corner of the screen at boot time. For reference, the AKI and AKI2G models are as follows: |
dusty.schafer |
English |
Sie wissen nicht, ob Sie einen Servo- oder Schrittmotor brauchen?
Die richtige Unterstützung für Sie
Haben Sie schon mal einen gehäuselosen Motor in Betracht gezogen?
Read MoreEntwickeln Sie außergewöhnliche Lösungen