The Cimrex 41 operator terminal (M.1302.74250 is obsolete and replaced by EXTER T40m (M.3000.0170) or T40t (M.3000.0171).
The T40m is a Graphic Touch operator terminal, 320x240 pixels, Backlit 3.5" TFT-LCD 16 greyscales
This article refers to G&L PiC application note and provides troubleshooting charts with logical and progressive methods for diagnosing a variety of problems that may occur with DS100 and DS200
This document refers to G&L PiC application note AN000019 and describes shunt power calculations for incremental motion applications. Applies to all G&L Centurion drives (DSM100, DS100, DS200, and AS100) and motors (SSM, FSM, and HSM).
This document refers to G&L PiC application note AN000018 and describes drive fuse sizing. Applies to all G&L Centurionä drives (DSM100, DS100, DS200, and AS100) and motors (SSM, FSM, and HSM).
This document refers to G&L PiC application note AN000017 and provides information on the sizing of the transformers for use with G&L Centurion Servo Drives (DSM100, DS100, DS200, and AS100) and motors (SSM, FSM, and HSM).
This PiC…
This document refers to G&L PiC application note AN000016 and describes running PiCServoPro/PiCPro on Windows 95.
The following procedure can be used to configure an MS-DOS session in Windows 95 to run PiCPro/PiCServoPro software. There is…
This article refers to G&L PiC application note AN000015 and describes analog input module initialization information.
The analog input module is used in conjunction with the functions A_INCHIT (analog input channel initialize), A_INCHRD…
This article refers to G&L PiC application note AN000014 and describes PiCPro library revision numbers.
The following table lists the version numbers of each library for each version of PiCPro. The version number can be identified by…