AKD1G vs AKD2G EtherNet/IP Command and Response Assembly StructureThe following chart demonstrates the differences in byte allocation for the command and response assemblies for the AKD1G and AKD2G EtherNet/IP drives. |
toddevans01 |
English | |
AKD Profinet PN.ACCSCALING ExamplesPN.ACCSCALING sets the scaling factor for acceleration rates related to PROFINET motion commands. The AKD PROFINET manual states that it applies to Jog Acc (PNU 1006), Jog Dec (PNU 1007), DRV_ACC (Telegram Signal 108), and DRV_DEC (Telegram Signal 109), and no other parameters. However… |
jcoleman02 |
English | |
Getting Started with PxMM UDP Communications - using Packet SenderThis application note uses the PC utility Packet Sender (download at https://packetsender.com/) to perform simple communications between a PxMM and a PC. The program “udpProgram” in the project UDP test Send-Receive First Transmission Each Way.kas has been added to a .kas… |
C Wontrop |
English | |
MLFB_HomeFindHomeInput with additional featuresThe KAS IDE comes with the UDFB (User-Defined Function Block) MLFB_HomeFindHomeInput. This post contains an updated version of the UDFB with the following changes: The homing sensor was used as normal detection, It is set to detect falling edge. After the home sensor is tripped… |
C Wontrop |
English | |
Grounding and Shielding Landing Page (Prevent Noise Issues)Broad best practices and resources for EMI best practices & troubleshooting. | kdn-adm |
English | |
AKD2G and KAS Functional Safety Landing Page This page contains information and links related to supporting functional safety in the AKD2G drive and KAS system. |
C Wontrop |
English | |
Migration from AKD EtherCAT IP mode to AKD2G CSP modeWhen migrating from AKD EtherCAT IP mode (Interpolated Position) to AKD2G EtherCAT CSP mode (Cyclic Synchronous Position), the only thing that needs to be changed is the target position object (change from 60C1h sub1 to 607Ah). |
jcoleman02 |
English | |
Sample KAS Project with Safety Controller Based Safety ParametersThis article contains 2 videos and presents sample code for a KAS Safety application with: SCU Safety PLC with SafePLC2 software (safety parameters defined with SafePLC2 software) PCMM Machine/Motion Controller AKD2G Servo Drive with FS3 card AKT2G Remote I/O Safety modules FSOE… |
C Wontrop |
English | |
KAS v3.07 is now available!!New Features Modular EtherCAT Topology AKT2G-BRC-000-000 - Brake chopper terminal Modify PLCopen axis user units from a program IDE Improvements For more details, please see the attached release note. |
dusty.schafer |
English |
Entre pas-à-pas et asservissement, votre cœur balance ?
Trouvez l'assistance dont vous avez besoin
Bobinages de moteurs : comprendre leur fonctionnement et leur influence sur les performances
Read MoreUne ingénierie exceptionnelle