Skip to main content

Kollmorgen Support Network

KAS IDE fails to load ESI files and display missing ESI files error messages when FIPS security policy is enabledKAS IDE fails to load the ESI files from the ESI library and fails to add the EtherCAT devices to the project when the FIPS (Federal Information Process Standards) security policy is enabled on the computer.
Prashanth Morishetty
English
Trade ComplianceKollmorgen is committed to sourcing components and materials from companies that share our values regarding respect for human rights, integrity and environmental responsibility.
Bethany Seymour
English
AKT and AKT2G Remote I/O ComparisonThe AKT2G family is recommended for new applications requiring remote I/O in a PCMM or PDMM KAS application. This article and attachment compares the AKT2G Remote I/O family with the AKT Remote I/O family.
Will Gaffga
English
(ABM)(3D Drawings) Altra Brasil Servo SeriesThese 3D models are intended to guide your design activities and can be used as reference information. Be sure to consult a Kollmorgen expert to ensure you have the most current and accurate information for critical aspects of the design work.
Leonardo Souza
English
(ABD & ABM) Altra Brasil Servo SeriesThe Altra Brasil Servo Series, consisting of the ABD® (Altra Brasil Drive) and ABM® (Altra Brasil Motor) series, is a complete line of EtherCAT-based servo drives developed specifically for the Brazilian market. With a high level of competitiveness and cost-effectiveness, it is integrated with…
Leonardo Souza
English
AKD2G Profinet PNU Reads and Writes Application Note Revision AThis application note demonstrates AKD2G parameter access from a S7-1500 PLC using the SinaPara function block for multi-parameter access and the SinaParaS for single parameter access.
toddevans01
English
KAS IDE v4.00 is now available!!New Features Next Generation Controller Software Compatible with PCMM/PDMM (1st Generation Controllers) 64-bit Runtime (2nd Generation Controllers) AKD2G Modular Device Profile (MDP) I/O MDP IO support for model variants
Prashanth Morishetty
English
KVB HMI - Displaying Bitwise Variables in KVB / AKI2GIntroduction KAS application developers can combine multiple pieces of information into one variable.
C Wontrop
English
First AKD2G TuningUsers facing the tuning of an AKD2G servodrive for the first time will have to use the Workbench configuration software tool which, for novice users or users of the Servostar series drive, may confuse them given the difference in the graphical interface and the many features introduced. This note…
Stefano Giacomelli Stefano Giacomelli
English