We have purchased a couple of AKD-P01206-NBCC-E000 drivers. We would like to power them only with 320V DC. It has been stated in the following link that we can supply DC voltage to L1 and L2 AC input terminals or DC bus terminals. But there…
Many servo applications exist in which it is more practical to use a DC power supply for the motor bus power instead of using AC power. Some of these include the use of batteries, generators, low voltage DC power supplies, and there are cases…